PatternClockingBuilderClockingType Enumeration

NXOpen.GeometricUtilities.PatternClockingBuilder.ClockingType is an alias for NXOpen.GeometricUtilities.PatternClockingBuilderClockingType

class NXOpen.GeometricUtilities.PatternClockingBuilderClockingType

Bases: object

type of pattern clocking to transform individual instances

Enum Members

Enum Member Enum Member Description
WithinPatternDefinitionLinear
WithinPatternDefinitionCircular
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.