PartModuleReferencesBuilder Class¶
-
class
NXOpen.GeometricUtilities.
PartModuleReferencesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.PartModuleReferencesBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ExpressionList | Returns the expressions for part module input/output |
GeometryList | Returns the geometric references for part module input/output |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ExpressionList¶
-
PartModuleReferencesBuilder.
ExpressionList
¶ Returns the expressions for part module input/output
-------------------------------------
Getter Method
Signature
ExpressionList
Returns: list of expressions Return type: NXOpen.SelectExpressionList
New in version NX8.0.0.
License requirements: None.
GeometryList¶
-
PartModuleReferencesBuilder.
GeometryList
¶ Returns the geometric references for part module input/output
-------------------------------------
Getter Method
Signature
GeometryList
Returns: list of geometries Return type: NXOpen.GeometricUtilities.SelectionListList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PartModuleReferencesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.