ParentEquivalencyMapType Enumeration¶
NXOpen.GeometricUtilities.ParentEquivalencyMap.Type is an alias for NXOpen.GeometricUtilities.ParentEquivalencyMapType
-
class
NXOpen.GeometricUtilities.
ParentEquivalencyMapType
¶ Bases:
object
enum for map type
Enum Members
Enum Member Enum Member Description Undefined undefined UserDefined user defined or manual NameBased mapped by name Geometric mapped by geometric comparison Inferred inferred from accepted Internal internal ID reuse Inherited inherited from other part or operation Mixed combination of multiple methods -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-