OrientXpressTestBuilderPlane Enumeration¶
NXOpen.GeometricUtilities.OrientXpressTestBuilder.Plane is an alias for NXOpen.GeometricUtilities.OrientXpressTestBuilderPlane
-
class
NXOpen.GeometricUtilities.
OrientXpressTestBuilderPlane
¶ Bases:
object
the active plane options
Enum Members
Enum Member Enum Member Description Xy Active plane is parallel to xy-plane Yz Active plane is parallel to yz-plane Xz Active plane is parallel to yz-plane NotSet Passive input mode -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-