OrientXpressTestBuilderAxisBlock Enumeration¶
NXOpen.GeometricUtilities.OrientXpressTestBuilder.AxisBlock is an alias for NXOpen.GeometricUtilities.OrientXpressTestBuilderAxisBlock
-
class
NXOpen.GeometricUtilities.
OrientXpressTestBuilderAxisBlock
¶ Bases:
object
the options to show or hide the axis block
Enum Members
Enum Member Enum Member Description Show Test show axis block Hide Test hide axis block -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-