ModlMotionOptions Enumeration¶
NXOpen.GeometricUtilities.ModlMotion.Options is an alias for NXOpen.GeometricUtilities.ModlMotionOptions
-
class
NXOpen.GeometricUtilities.
ModlMotionOptions
¶ Bases:
object
Represents the options of Motion.
Enum Members
Enum Member Enum Member Description AlongCurveAngle Move by AlongCurve-Angle DistanceAngle Move by Distance-Angle Distance Move by Distance Angle Move by Angle DistanceBetweenPoints Move by Distance between Points RadialDistance Move by Radial Distance PointToPoint Move by Point to Point RotateByThreePoints Move by Rotate by Three Points AlignAxisVector Move by Align Axis to Vector CsysToCsys Move by CSYS to CSYS Dynamic Move by Dynamic DeltaXyz Move by delta XYZ NotSet No move -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-