MiddleHoleData Class¶
-
class
NXOpen.GeometricUtilities.
MiddleHoleData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.MiddleHoleData
New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
BooleanOperation | Returns the boolean operation |
EndChamferAngle | Returns the end chamfer angle |
EndChamferEnabled | Returns or sets the end chamfer enabled |
EndChamferOffset | Returns the end chamfer offset |
FitOption | Returns or sets the fit option |
HoleDiameter | Returns the hole diameter |
MatchDimOfStartHole | Returns or sets the match dim of start hole |
StartChamferAngle | Returns the start chamfer angle |
StartChamferEnabled | Returns or sets the start chamfer enabled |
StartChamferOffset | Returns the start chamfer offset |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BooleanOperation¶
-
MiddleHoleData.
BooleanOperation
¶ Returns the boolean operation
-------------------------------------
Getter Method
Signature
BooleanOperation
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX5.0.2.
License requirements: None.
EndChamferAngle¶
-
MiddleHoleData.
EndChamferAngle
¶ Returns the end chamfer angle
-------------------------------------
Getter Method
Signature
EndChamferAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
EndChamferEnabled¶
-
MiddleHoleData.
EndChamferEnabled
¶ Returns or sets the end chamfer enabled
-------------------------------------
Getter Method
Signature
EndChamferEnabled
Returns: Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndChamferEnabled
Parameters: endChamferEnabled (bool) – New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
EndChamferOffset¶
-
MiddleHoleData.
EndChamferOffset
¶ Returns the end chamfer offset
-------------------------------------
Getter Method
Signature
EndChamferOffset
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
FitOption¶
-
MiddleHoleData.
FitOption
¶ Returns or sets the fit option
-------------------------------------
Getter Method
Signature
FitOption
Returns: Return type: str New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FitOption
Parameters: fitOption (str) – New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
HoleDiameter¶
-
MiddleHoleData.
HoleDiameter
¶ Returns the hole diameter
-------------------------------------
Getter Method
Signature
HoleDiameter
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
MatchDimOfStartHole¶
-
MiddleHoleData.
MatchDimOfStartHole
¶ Returns or sets the match dim of start hole
-------------------------------------
Getter Method
Signature
MatchDimOfStartHole
Returns: Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatchDimOfStartHole
Parameters: matchDimOfStartHole (bool) – New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
StartChamferAngle¶
-
MiddleHoleData.
StartChamferAngle
¶ Returns the start chamfer angle
-------------------------------------
Getter Method
Signature
StartChamferAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
StartChamferEnabled¶
-
MiddleHoleData.
StartChamferEnabled
¶ Returns or sets the start chamfer enabled
-------------------------------------
Getter Method
Signature
StartChamferEnabled
Returns: Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartChamferEnabled
Parameters: startChamferEnabled (bool) – New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
StartChamferOffset¶
-
MiddleHoleData.
StartChamferOffset
¶ Returns the start chamfer offset
-------------------------------------
Getter Method
Signature
StartChamferOffset
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
Method Detail¶
Validate¶
-
MiddleHoleData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.