LinearLimits Class

class NXOpen.GeometricUtilities.LinearLimits

Bases: NXOpen.GeometricUtilities.Limits

Represents a limits data.

New in version NX4.0.0.

Properties

Property Description
EndExtend Returns the end extend builder
StartExtend Returns the start extend builder
SymmetricOption Returns or sets the symmetric option
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Validate

LinearLimits.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.