InstanceEditedExpressionsList Class¶
-
class
NXOpen.GeometricUtilities.
InstanceEditedExpressionsList
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
list of
NXOpen.GeometricUtilities.InstanceEditedExpressionItem
objects.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
List | Returns the list of NXOpen.GeometricUtilities.InstanceEditedExpressionItem objects. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
EditInstanceExpression | This is the default creator for NXOpen.GeometricUtilities.InstanceEditedExpressionItem . |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
List¶
-
InstanceEditedExpressionsList.
List
¶ Returns the list of
NXOpen.GeometricUtilities.InstanceEditedExpressionItem
objects.-------------------------------------
Getter Method
Signature
List
Returns: Return type: NXOpen.GeometricUtilities.InstanceEditedExpressionItemList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
EditInstanceExpression¶
-
InstanceEditedExpressionsList.
EditInstanceExpression
¶ Overloaded method EditInstanceExpression
EditInstanceExpression()
EditInstanceExpression(masterExpression, instanceExpression)
-------------------------------------
This is the default creator for
NXOpen.GeometricUtilities.InstanceEditedExpressionItem
.Signature
EditInstanceExpression()
Returns: Return type: NXOpen.GeometricUtilities.InstanceEditedExpressionItem
New in version NX7.5.0.
License requirements: None.
-------------------------------------
This is the creator for
NXOpen.GeometricUtilities.InstanceEditedExpressionItem
which should be used.Signature
EditInstanceExpression(masterExpression, instanceExpression)
Parameters: - masterExpression (
NXOpen.Expression
) – the master expression - instanceExpression (
NXOpen.Expression
) – the instance expression
Returns: Return type: New in version NX7.5.0.
License requirements: None.
-------------------------------------
Validate¶
-
InstanceEditedExpressionsList.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.