HelixPatternSizeOptions Enumeration¶
NXOpen.GeometricUtilities.HelixPattern.SizeOptions is an alias for NXOpen.GeometricUtilities.HelixPatternSizeOptions
-
class
NXOpen.GeometricUtilities.
HelixPatternSizeOptions
¶ Bases:
object
defines Helix size options for Helix type pattern.
Enum Members
Enum Member Enum Member Description CountAngleDistance use Count, Angle, Distance to define a Helix CountHelixPitchAndTurns use Count, Helix Pitch, Turns to define a Helix CountHelixPitchAndSpan use Count, Helix Pitch, Span to define a Helix AngleHelixPitchAndTurns use Angle, Helix Pitch, Turns to define a Helix AngleHelixPitchAndSpan use Angle, Helix Pitch, Span to define a Helix -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-