GeometryLocationDataEntityTypes Enumeration

NXOpen.GeometricUtilities.GeometryLocationData.EntityTypes is an alias for NXOpen.GeometricUtilities.GeometryLocationDataEntityTypes

class NXOpen.GeometricUtilities.GeometryLocationDataEntityTypes

Bases: object

Represents the entity type.

Enum Members

Enum Member Enum Member Description
Point
Csys
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.