GeneralPattern Class¶
-
class
NXOpen.GeometricUtilities.
GeneralPattern
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
the General pattern definition.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
FromLocationCsys2d | Returns the from location 2d csys |
FromLocationCsys3d | Returns or sets the from location 3d csys |
FromLocationPoint | Returns or sets the from location point |
FromLocationType | Returns or sets the from location type |
Tag | Returns the Tag for this object. |
ToCsysList | Returns the to csys list |
ToPoints | Returns the to points |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GeneralPatternFromLocationOptions Enumeration | the from location options. |
Property Detail¶
FromLocationCsys2d¶
-
GeneralPattern.
FromLocationCsys2d
¶ Returns the from location 2d csys
-------------------------------------
Getter Method
Signature
FromLocationCsys2d
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.0.0.
License requirements: None.
FromLocationCsys3d¶
-
GeneralPattern.
FromLocationCsys3d
¶ Returns or sets the from location 3d csys
-------------------------------------
Getter Method
Signature
FromLocationCsys3d
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromLocationCsys3d
Parameters: csys ( NXOpen.CoordinateSystem
) –New in version NX8.0.0.
License requirements: None.
FromLocationPoint¶
-
GeneralPattern.
FromLocationPoint
¶ Returns or sets the from location point
-------------------------------------
Getter Method
Signature
FromLocationPoint
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromLocationPoint
Parameters: point ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: None.
FromLocationType¶
-
GeneralPattern.
FromLocationType
¶ Returns or sets the from location type
-------------------------------------
Getter Method
Signature
FromLocationType
Returns: Return type: NXOpen.GeometricUtilities.GeneralPatternFromLocationOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromLocationType
Parameters: fromLocationType ( NXOpen.GeometricUtilities.GeneralPatternFromLocationOptions
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ToCsysList¶
-
GeneralPattern.
ToCsysList
¶ Returns the to csys list
-------------------------------------
Getter Method
Signature
ToCsysList
Returns: Return type: NXOpen.SelectCoordinateSystemList
New in version NX8.0.0.
License requirements: None.
ToPoints¶
-
GeneralPattern.
ToPoints
¶ Returns the to points
-------------------------------------
Getter Method
Signature
ToPoints
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
GeneralPattern.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.