FacePlaneToolBuilder Class¶
-
class
NXOpen.GeometricUtilities.
FacePlaneToolBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
a sub-component of BooleanToolBuilder.
It provides two basic tools * creation methods i.e. collector sets of faces/datum planes, or a new plane * created on the fly.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ToolFaces | Returns the sets of tool faces or datum planes |
ToolPlane | Returns or sets the new plane created on the fly. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ToolFaces¶
-
FacePlaneToolBuilder.
ToolFaces
¶ Returns the sets of tool faces or datum planes
-------------------------------------
Getter Method
Signature
ToolFaces
Returns: Return type: NXOpen.GeometricUtilities.FaceSetData
New in version NX6.0.0.
License requirements: None.
ToolPlane¶
-
FacePlaneToolBuilder.
ToolPlane
¶ Returns or sets the new plane created on the fly.
Note: only one plane is get/set
-------------------------------------
Getter Method
Signature
ToolPlane
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolPlane
Parameters: toolPlane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
FacePlaneToolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.