ExtrudeRevolveToolBuilder Class¶
-
class
NXOpen.GeometricUtilities.
ExtrudeRevolveToolBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
a class which is a sub-component of BooleanTool.
It provides other two basic tools * creation methods by creating extrude or revolve bodies on the fly. Given a * super section with non-intersecting loops and a certain direction, * it will create a revolve tool or an extrude tool to do the boolean operation.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ToolAxis | Returns or sets the tool axis used for doing revolve |
ToolDirection | Returns or sets the tool direction used for doing extrude |
ToolSection | Returns the tool super section |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ToolAxis¶
-
ExtrudeRevolveToolBuilder.
ToolAxis
¶ Returns or sets the tool axis used for doing revolve
-------------------------------------
Getter Method
Signature
ToolAxis
Returns: Return type: NXOpen.Axis
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxis
Parameters: toolAxis ( NXOpen.Axis
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ToolDirection¶
-
ExtrudeRevolveToolBuilder.
ToolDirection
¶ Returns or sets the tool direction used for doing extrude
-------------------------------------
Getter Method
Signature
ToolDirection
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolDirection
Parameters: toolDirection ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ToolSection¶
-
ExtrudeRevolveToolBuilder.
ToolSection
¶ Returns the tool super section
-------------------------------------
Getter Method
Signature
ToolSection
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ExtrudeRevolveToolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.