ExtensionSide Enumeration¶
-
class
NXOpen.GeometricUtilities.
ExtensionSide
¶ Bases:
object
This enum represents the extension side Enum Members
Enum Member Enum Member Description StartEnd Extension Side Start/End Start Extension Side Start End Extension Side End Symmetric Extension Side Symmetric -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-