ExtendExtendType Enumeration

NXOpen.GeometricUtilities.Extend.ExtendType is an alias for NXOpen.GeometricUtilities.ExtendExtendType

class NXOpen.GeometricUtilities.ExtendExtendType

Bases: object

This enum represents the type of extend

Enum Members

Enum Member Enum Member Description
Value
UntilNext
UntilSelected
UntilExtended
ThroughAll
Symmetric
Percent
ArcLength
ThruPoint
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.