EnumTestConstraints Enumeration¶
NXOpen.GeometricUtilities.EnumTest.Constraints is an alias for NXOpen.GeometricUtilities.EnumTestConstraints
-
class
NXOpen.GeometricUtilities.
EnumTestConstraints
¶ Bases:
object
constraints are rather smelly
Enum Members
Enum Member Enum Member Description Coincident coincident constraints are not coincidental Parallel parallel constraints can run serially Colinear colinear constraints can’t run parallel Concentric concentric constraints are… ah, screw it EqualRadius I’m giving up Fixed ahhhhh, it’s over -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-