EndHoleDataThreadRotationOptions Enumeration¶
NXOpen.GeometricUtilities.EndHoleData.ThreadRotationOptions is an alias for NXOpen.GeometricUtilities.EndHoleDataThreadRotationOptions
-
class
NXOpen.GeometricUtilities.
EndHoleDataThreadRotationOptions
¶ Bases:
object
Represents thread rotation options.
Enum Members
Enum Member Enum Member Description Right Right rotation Left Left rotation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-