EndHoleDataHoleDepthOptions Enumeration

NXOpen.GeometricUtilities.EndHoleData.HoleDepthOptions is an alias for NXOpen.GeometricUtilities.EndHoleDataHoleDepthOptions

class NXOpen.GeometricUtilities.EndHoleDataHoleDepthOptions

Bases: object

Represents hole depth specification options.

Enum Members

Enum Member Enum Member Description
ToCylinderBottom
ToConeTip
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.