CurveOptionsInputCurve Enumeration¶
NXOpen.GeometricUtilities.CurveOptions.InputCurve is an alias for NXOpen.GeometricUtilities.CurveOptionsInputCurve
-
class
NXOpen.GeometricUtilities.
CurveOptionsInputCurve
¶ Bases:
object
Represents the input curve options
Enum Members
Enum Member Enum Member Description Retain Retains the original input curve and creates the new output curve Blank Blanks the original input curve and creates the new output curve Delete Deletes the original input curve and creates the new output curve Replace Replaces the original input curve with the new output curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-