CurveLengthBuilder Class¶
-
class
NXOpen.GeometricUtilities.
CurveLengthBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.CurveLengthBuilder
builderNew in version NX12.0.0.
Properties¶
Property | Description |
---|---|
EndOffset0 | Returns the end 1 length |
EndOffset1 | Returns the end 2 length |
EndSelection0 | Returns the select object for end 1 |
EndSelection1 | Returns the select object for end 2 |
EndType0 | Returns or sets the end 1 type |
EndType1 | Returns or sets the end 2 type |
ReverseEndOffset0Direction | Returns or sets the reverse endOffset0 direction flag. |
ReverseEndOffset1Direction | Returns or sets the reverse endOffset1 direction flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CurveLengthBuilderEndObjectType Enumeration | This attribute represents end type |
Property Detail¶
EndOffset0¶
-
CurveLengthBuilder.
EndOffset0
¶ Returns the end 1 length
-------------------------------------
Getter Method
Signature
EndOffset0
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
EndOffset1¶
-
CurveLengthBuilder.
EndOffset1
¶ Returns the end 2 length
-------------------------------------
Getter Method
Signature
EndOffset1
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
EndSelection0¶
-
CurveLengthBuilder.
EndSelection0
¶ Returns the select object for end 1
-------------------------------------
Getter Method
Signature
EndSelection0
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX12.0.0.
License requirements: None.
EndSelection1¶
-
CurveLengthBuilder.
EndSelection1
¶ Returns the select object for end 2
-------------------------------------
Getter Method
Signature
EndSelection1
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX12.0.0.
License requirements: None.
EndType0¶
-
CurveLengthBuilder.
EndType0
¶ Returns or sets the end 1 type
-------------------------------------
Getter Method
Signature
EndType0
Returns: Return type: NXOpen.GeometricUtilities.CurveLengthBuilderEndObjectType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndType0
Parameters: endType0 ( NXOpen.GeometricUtilities.CurveLengthBuilderEndObjectType
) –New in version NX12.0.0.
License requirements: None.
EndType1¶
-
CurveLengthBuilder.
EndType1
¶ Returns or sets the end 2 type
-------------------------------------
Getter Method
Signature
EndType1
Returns: Return type: NXOpen.GeometricUtilities.CurveLengthBuilderEndObjectType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndType1
Parameters: endType1 ( NXOpen.GeometricUtilities.CurveLengthBuilderEndObjectType
) –New in version NX12.0.0.
License requirements: None.
ReverseEndOffset0Direction¶
-
CurveLengthBuilder.
ReverseEndOffset0Direction
¶ Returns or sets the reverse endOffset0 direction flag.
Indicates whether the endOffset0 direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseEndOffset0Direction
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseEndOffset0Direction
Parameters: reverseEndOffset0Direction (bool) – New in version NX12.0.0.
License requirements: None.
ReverseEndOffset1Direction¶
-
CurveLengthBuilder.
ReverseEndOffset1Direction
¶ Returns or sets the reverse endOffset1 direction flag.
Indicates whether the endOffset1 direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseEndOffset1Direction
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseEndOffset1Direction
Parameters: reverseEndOffset1Direction (bool) – New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CurveLengthBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.