CurveFitDataMethod Enumeration¶
NXOpen.GeometricUtilities.CurveFitData.Method is an alias for NXOpen.GeometricUtilities.CurveFitDataMethod
-
class
NXOpen.GeometricUtilities.
CurveFitDataMethod
¶ Bases:
object
Represents the curve fitting method in the case of advanced fitting
Enum Members
Enum Member Enum Member Description DegreeAndSegments Degree and Segments DegreeAndTolerance Degree and Tolerance KeepParameterization Keep Parameterization AutoFit Auto Fit -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-