CurveExtendData Class¶
-
class
NXOpen.GeometricUtilities.
CurveExtendData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.CurveExtendData
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns the distance |
LimitOption | Returns or sets the limit option |
Tag | Returns the Tag for this object. |
UntilSelectedObject | Returns the until selected object |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CurveExtendDataLimitOptions Enumeration | Represents the curve extend options for associative basic curves |
Property Detail¶
Distance¶
-
CurveExtendData.
Distance
¶ Returns the distance
-------------------------------------
Getter Method
Signature
Distance
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
LimitOption¶
-
CurveExtendData.
LimitOption
¶ Returns or sets the limit option
-------------------------------------
Getter Method
Signature
LimitOption
Returns: Return type: NXOpen.GeometricUtilities.CurveExtendDataLimitOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitOption
Parameters: limitOption ( NXOpen.GeometricUtilities.CurveExtendDataLimitOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
UntilSelectedObject¶
-
CurveExtendData.
UntilSelectedObject
¶ Returns the until selected object
-------------------------------------
Getter Method
Signature
UntilSelectedObject
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CurveExtendData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.