CircularCrossSection Class¶
-
class
NXOpen.GeometricUtilities.
CircularCrossSection
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a circular section data for face blend.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
LawControl | Returns the Law builder |
Radius | Returns the radius for the circular section with face blend |
RadiusOption | Returns or sets the radius option for the circular section with face blend |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
SetLawControlConstantRadius | Sets a constant radius for the law control of the circular section with face blend. |
SetLawControlEndRadius | Sets a end radius for the law control of the circular section with face blend. |
SetLawControlStartRadius | Sets a start radius for the law control of the circular section with face blend. |
SetRadius | Sets a radius for the circular section with face blend. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LawControl¶
-
CircularCrossSection.
LawControl
¶ Returns the Law builder
-------------------------------------
Getter Method
Signature
LawControl
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX5.0.0.
License requirements: None.
Radius¶
-
CircularCrossSection.
Radius
¶ Returns the radius for the circular section with face blend
-------------------------------------
Getter Method
Signature
Radius
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
RadiusOption¶
-
CircularCrossSection.
RadiusOption
¶ Returns or sets the radius option for the circular section with face blend
-------------------------------------
Getter Method
Signature
RadiusOption
Returns: Return type: NXOpen.GeometricUtilities.RadiusMethod
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusOption
Parameters: method ( NXOpen.GeometricUtilities.RadiusMethod
) –New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
SetLawControlConstantRadius¶
-
CircularCrossSection.
SetLawControlConstantRadius
¶ Sets a constant radius for the law control of the circular section with face blend.
Signature
SetLawControlConstantRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlEndRadius¶
-
CircularCrossSection.
SetLawControlEndRadius
¶ Sets a end radius for the law control of the circular section with face blend.
Signature
SetLawControlEndRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlStartRadius¶
-
CircularCrossSection.
SetLawControlStartRadius
¶ Sets a start radius for the law control of the circular section with face blend.
Signature
SetLawControlStartRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetRadius¶
-
CircularCrossSection.
SetRadius
¶ Sets a radius for the circular section with face blend.
Signature
SetRadius(radius)
Parameters: radius (str) – New in version NX4.0.0.
Deprecated since version NX9.0.0: To set the value of the expression modify the expression directly using
GeometricUtilities.CircularCrossSection.Radius()
andExpression.RightHandSide()
.License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
CircularCrossSection.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.