BoundingObjectBuilderMethod Enumeration¶
NXOpen.GeometricUtilities.BoundingObjectBuilder.Method is an alias for NXOpen.GeometricUtilities.BoundingObjectBuilderMethod
-
class
NXOpen.GeometricUtilities.
BoundingObjectBuilderMethod
¶ Bases:
object
Represents Bounding Object option types.
Enum Members
Enum Member Enum Member Description ExistingCurve Existing Curve ProjectPoint Project Point LineBy2Points Line by 2 Points PointAndVector Point and Vector ByPlane By Plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-