BooleanToolBuilderBooleanToolType Enumeration¶
NXOpen.GeometricUtilities.BooleanToolBuilder.BooleanToolType is an alias for NXOpen.GeometricUtilities.BooleanToolBuilderBooleanToolType
-
class
NXOpen.GeometricUtilities.
BooleanToolBuilderBooleanToolType
¶ Bases:
object
the boolean tool created options
Enum Members
Enum Member Enum Member Description FaceOrPlane Tool consists of sets of faces or datum planes NewPlane Tool consists of plane created on the fly Extrude Tool consists of extrude created on the fly Revolve Tool consists of revolve created on the fly -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-