BooleanOperationBooleanType Enumeration¶
NXOpen.GeometricUtilities.BooleanOperation.BooleanType is an alias for NXOpen.GeometricUtilities.BooleanOperationBooleanType
-
class
NXOpen.GeometricUtilities.
BooleanOperationBooleanType
¶ Bases:
object
Boolean operation type.
Enum Members
Enum Member Enum Member Description Create Create Unite Unite Subtract Subtract Intersect Intersect Sew Sew -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-