BlendSetbackBuilderDirections Enumeration¶
NXOpen.GeometricUtilities.BlendSetbackBuilder.Directions is an alias for NXOpen.GeometricUtilities.BlendSetbackBuilderDirections
-
class
NXOpen.GeometricUtilities.
BlendSetbackBuilderDirections
¶ Bases:
object
Setback direction options
Enum Members
Enum Member Enum Member Description U setback curve is an iso-u parameter curve V setback curve is an iso-v parameter curve Plane setback curve is the intersection curve between a plane and faces -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-