AngularLimits Class

class NXOpen.GeometricUtilities.AngularLimits

Bases: NXOpen.GeometricUtilities.Limits

Represents a angular limts data.

New in version NX3.0.1.

Properties

Property Description
Distance Returns a computed distance
EndExtend Returns the end extend builder
StartExtend Returns the start extend builder
SymmetricOption Returns or sets the symmetric option
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Distance

AngularLimits.Distance

Returns a computed distance

-------------------------------------

Getter Method

Signature Distance

Returns:
Return type:float

New in version NX3.0.1.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

AngularLimits.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.