AlongPathPatternYDirectionOptions Enumeration¶
NXOpen.GeometricUtilities.AlongPathPattern.YDirectionOptions is an alias for NXOpen.GeometricUtilities.AlongPathPatternYDirectionOptions
-
class
NXOpen.GeometricUtilities.
AlongPathPatternYDirectionOptions
¶ Bases:
object
This defines y direction Types
Enum Members
Enum Member Enum Member Description Vector y direction is a vector. Section y direction is a section. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-