AlongPathPatternPathOptions Enumeration¶
NXOpen.GeometricUtilities.AlongPathPattern.PathOptions is an alias for NXOpen.GeometricUtilities.AlongPathPatternPathOptions
-
class
NXOpen.GeometricUtilities.
AlongPathPatternPathOptions
¶ Bases:
object
This defines path options
Enum Members
Enum Member Enum Member Description Rigid path is the selected section. Offset path is an offset from the selected path. Translate path is a translation from the selected path. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-