AlignmentMethodBuilderType Enumeration

NXOpen.GeometricUtilities.AlignmentMethodBuilder.Type is an alias for NXOpen.GeometricUtilities.AlignmentMethodBuilderType

class NXOpen.GeometricUtilities.AlignmentMethodBuilderType

Bases: object

Alignment types supported

Enum Members

Enum Member Enum Member Description
Parameter
ArcLength
Points
Distance
Angle
SpineCurve
SplinePoints
Segments
Developable
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.