SimpleInterferenceResult Enumeration¶
NXOpen.GeometricAnalysis.SimpleInterference.Result is an alias for NXOpen.GeometricAnalysis.SimpleInterferenceResult
-
class
NXOpen.GeometricAnalysis.
SimpleInterferenceResult
¶ Bases:
object
Specifies the result of a simple interference check
Enum Members
Enum Member Enum Member Description NoInterference No interference exists between the input bodies. OnlyEdgesOrFacesInterfere Only faces or edges interfere and no solid interference exists between the input bodies. InterferenceExists Interference exists between the input bodies. Use NXOpen.GeometricAnalysis.SimpleInterference.GetInterferenceResults()
to obtain the pairs of faces interfering or interference solid(s) created between the input bodies.CanNotPerformCheck An unknown error has occured while performing the interference check. Check could not be performed between the input bodies. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-