SimpleInterferenceFaceInterferenceMethod Enumeration¶
NXOpen.GeometricAnalysis.SimpleInterference.FaceInterferenceMethod is an alias for NXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod
-
class
NXOpen.GeometricAnalysis.
SimpleInterferenceFaceInterferenceMethod
¶ Bases:
object
Specifies to “find only first pair of interfering faces” or “all pairs of interfering faces” between the input boides.
Enum Members
Enum Member Enum Member Description FirstPairOnly Find first pair of interfering faces AllPairs Find all pairs of interfering faces. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-