SectionPlaneBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
SectionPlaneBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a plane which is used to cut sections on faces or facet bodies
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
Origin | Returns or sets the plane origin |
Plane | Returns or sets the plane type |
Tag | Returns the Tag for this object. |
XAxis | Returns or sets the plane X axis |
YAxis | Returns or sets the plane Y axis |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SectionPlaneBuilderPlaneType Enumeration | The type of different section planes |
Property Detail¶
Origin¶
-
SectionPlaneBuilder.
Origin
¶ Returns or sets the plane origin
-------------------------------------
Getter Method
Signature
Origin
Returns: Return type: NXOpen.Point3d
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Origin
Parameters: origin ( NXOpen.Point3d
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Plane¶
-
SectionPlaneBuilder.
Plane
¶ Returns or sets the plane type
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilderPlaneType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilderPlaneType
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
XAxis¶
-
SectionPlaneBuilder.
XAxis
¶ Returns or sets the plane X axis
-------------------------------------
Getter Method
Signature
XAxis
Returns: Return type: NXOpen.Vector3d
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XAxis
Parameters: xAxis ( NXOpen.Vector3d
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
YAxis¶
-
SectionPlaneBuilder.
YAxis
¶ Returns or sets the plane Y axis
-------------------------------------
Getter Method
Signature
YAxis
Returns: Return type: NXOpen.Vector3d
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YAxis
Parameters: yAxis ( NXOpen.Vector3d
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
Validate¶
-
SectionPlaneBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.