SectionAnalysisExBuilderPlacementType Enumeration¶
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.PlacementType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderPlacementType
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
SectionAnalysisExBuilderPlacementType
¶ Bases:
object
The types of the section placement
Enum Members
Enum Member Enum Member Description Uniform Uniformly distributed ThroughPoints Through the specified points BetweenPoints Distributed between two specified points Interactive Interactively specified -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-