SectionAnalysisExBuilderAlignmentType Enumeration¶
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.AlignmentType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
SectionAnalysisExBuilderAlignmentType
¶ Bases:
object
The section alignment type
Enum Members
Enum Member Enum Member Description XYZPlane The cutting planes are perpendicular to X, Y or Z plane ParallelPlanes The cutting planes are parallel to a specified plane CurveAligned The cutting planes are perpendicular to specified curves Isoparametric The sections are along isoparametric lines Radial The cutting planes are distributed along a circle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-