RadialBuilderRotationAxisType Enumeration¶
NXOpen.GeometricAnalysis.SectionAnalysis.RadialBuilder.RotationAxisType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.RadialBuilderRotationAxisType
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
RadialBuilderRotationAxisType
¶ Bases:
object
The type of the rotation axis
Enum Members
Enum Member Enum Member Description Xc XC axis Yc YC axis Zc ZC axis View View direction ArbitraryVector A user specified vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-