IsoparametricBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
IsoparametricBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Isoparametric specification for a
GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder
.New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
IsSpacingEnabled | Returns or sets a value indicating whether the spacing is applied |
IsUEnabled | Returns or sets a value indicating wheter the U direction is enabled |
IsVEnabled | Returns or sets a value indicating wheter the V direction is enabled |
Number | Returns or sets a value indicating how many sections should be created |
Spacing | Returns or sets a value indicating the space between sections |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
IsSpacingEnabled¶
-
IsoparametricBuilder.
IsSpacingEnabled
¶ Returns or sets a value indicating whether the spacing is applied
-------------------------------------
Getter Method
Signature
IsSpacingEnabled
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSpacingEnabled
Parameters: isSpacingEnabled (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
IsUEnabled¶
-
IsoparametricBuilder.
IsUEnabled
¶ Returns or sets a value indicating wheter the U direction is enabled
-------------------------------------
Getter Method
Signature
IsUEnabled
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsUEnabled
Parameters: isUEnabled (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
IsVEnabled¶
-
IsoparametricBuilder.
IsVEnabled
¶ Returns or sets a value indicating wheter the V direction is enabled
-------------------------------------
Getter Method
Signature
IsVEnabled
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsVEnabled
Parameters: isVEnabled (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Number¶
-
IsoparametricBuilder.
Number
¶ Returns or sets a value indicating how many sections should be created
-------------------------------------
Getter Method
Signature
Number
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Number
Parameters: number (int) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Spacing¶
-
IsoparametricBuilder.
Spacing
¶ Returns or sets a value indicating the space between sections
-------------------------------------
Getter Method
Signature
Spacing
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Spacing
Parameters: spacing (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
Validate¶
-
IsoparametricBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.