InteractiveBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
InteractiveBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Interactive specification for a
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder
.New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
InteractiveSection | Returns the interactive section lines |
IsCutInfiniteEnabled | Returns or sets a value indicating whether extending the interactive section lines to infinite |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
InteractiveSection¶
-
InteractiveBuilder.
InteractiveSection
¶ Returns the interactive section lines
-------------------------------------
Getter Method
Signature
InteractiveSection
Returns: Return type: NXOpen.GeometricUtilities.InteractiveSectionBuilder
New in version NX7.0.0.
License requirements: None.
IsCutInfiniteEnabled¶
-
InteractiveBuilder.
IsCutInfiniteEnabled
¶ Returns or sets a value indicating whether extending the interactive section lines to infinite
-------------------------------------
Getter Method
Signature
IsCutInfiniteEnabled
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCutInfiniteEnabled
Parameters: enabled (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
Validate¶
-
InteractiveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.