GridSpacingBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
GridSpacingBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the grid spacing for certain types of section specifications for the
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder
.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BoundSections1 | Returns or sets the flag to bound the section to grid in direction 1 |
BoundSections2 | Returns or sets the flag to bound the section to grid in direction 2 |
Interval1 | Returns or sets the interval of sections in direction 1 |
Interval2 | Returns or sets the interval of sections in direction 2 |
LockInterval1 | Returns or sets the flag to lock the section interval in direction 1 |
LockInterval2 | Returns or sets the flag to lock the section interval in direction 2 |
SectionNumber1 | Returns or sets the number of sections in direction 1 |
SectionNumber2 | Returns or sets the number of sections in direction 2 |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BoundSections1¶
-
GridSpacingBuilder.
BoundSections1
¶ Returns or sets the flag to bound the section to grid in direction 1
-------------------------------------
Getter Method
Signature
BoundSections1
Returns: Return type: bool New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
BoundSections1
Parameters: boundSections1 (bool) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
BoundSections2¶
-
GridSpacingBuilder.
BoundSections2
¶ Returns or sets the flag to bound the section to grid in direction 2
-------------------------------------
Getter Method
Signature
BoundSections2
Returns: Return type: bool New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
BoundSections2
Parameters: boundSections2 (bool) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Interval1¶
-
GridSpacingBuilder.
Interval1
¶ Returns or sets the interval of sections in direction 1
-------------------------------------
Getter Method
Signature
Interval1
Returns: Return type: float New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
Interval1
Parameters: interval1 (float) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Interval2¶
-
GridSpacingBuilder.
Interval2
¶ Returns or sets the interval of sections in direction 2
-------------------------------------
Getter Method
Signature
Interval2
Returns: Return type: float New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
Interval2
Parameters: interval2 (float) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
LockInterval1¶
-
GridSpacingBuilder.
LockInterval1
¶ Returns or sets the flag to lock the section interval in direction 1
-------------------------------------
Getter Method
Signature
LockInterval1
Returns: Return type: bool New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
LockInterval1
Parameters: lockInterval1 (bool) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
LockInterval2¶
-
GridSpacingBuilder.
LockInterval2
¶ Returns or sets the flag to lock the section interval in direction 2
-------------------------------------
Getter Method
Signature
LockInterval2
Returns: Return type: bool New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
LockInterval2
Parameters: lockInterval2 (bool) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SectionNumber1¶
-
GridSpacingBuilder.
SectionNumber1
¶ Returns or sets the number of sections in direction 1
-------------------------------------
Getter Method
Signature
SectionNumber1
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
SectionNumber1
Parameters: sectionNumber1 (int) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SectionNumber2¶
-
GridSpacingBuilder.
SectionNumber2
¶ Returns or sets the number of sections in direction 2
-------------------------------------
Getter Method
Signature
SectionNumber2
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
-------------------------------------
Setter Method
Signature
SectionNumber2
Parameters: sectionNumber2 (int) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
Validate¶
-
GridSpacingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.