ReflectionAnalysisBuilderNumberOfLinesOptions Enumeration¶
NXOpen.GeometricAnalysis.ReflectionAnalysisBuilder.NumberOfLinesOptions is an alias for NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderNumberOfLinesOptions
-
class
NXOpen.GeometricAnalysis.
ReflectionAnalysisBuilderNumberOfLinesOptions
¶ Bases:
object
The number of reflection lines.
Enum Members
Enum Member Enum Member Description One 1 reflection line. Two 2 reflection line. Four 4 reflection line. Eight 8 reflection line. Sixteen 16 reflection line. ThirtyTwo 32 reflection line. SixtyFour 64 reflection line. OneTwoEight 128 reflection line. TwoFiveSix 256 reflection line. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-