RadiusAnalysisBuilderTypes Enumeration¶
NXOpen.GeometricAnalysis.RadiusAnalysisBuilder.Types is an alias for NXOpen.GeometricAnalysis.RadiusAnalysisBuilderTypes
-
class
NXOpen.GeometricAnalysis.
RadiusAnalysisBuilderTypes
¶ Bases:
object
Represents the radius type.
Enum Members
Enum Member Enum Member Description Gaussian Gaussian radius. Minimum Minimum radius. Maximum Maximum radius. Mean Mean radius. Normal Normal radius. Sectional Sectional radius. U Radius in U direction. V Radius in V direction. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-