ExamineGeometryCheck Enumeration¶
NXOpen.GeometricAnalysis.ExamineGeometry.Check is an alias for NXOpen.GeometricAnalysis.ExamineGeometryCheck
-
class
NXOpen.GeometricAnalysis.
ExamineGeometryCheck
¶ Bases:
object
Types of checks
Enum Members
Enum Member Enum Member Description ObjectTiny ObjectTiny ObjectMisaligned ObjectMisaligned BodyDataStructures BodyDataStructures BodyConsistency BodyConsistency BodyFaceIntersections BodyFaceIntersections BodySheetBoundaries BodySheetBoundaries FaceSmoothness FaceSmoothness FaceSelfIntersection FaceSelfIntersection FaceSpikesCuts FaceSpikesCuts EdgeSmoothness EdgeSmoothness EdgeTolerances EdgeTolerances NumChecks Number of Checks -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-