DeviationGaugeBuilderXyzDirectionType Enumeration¶
NXOpen.GeometricAnalysis.DeviationGaugeBuilder.XyzDirectionType is an alias for NXOpen.GeometricAnalysis.DeviationGaugeBuilderXyzDirectionType
-
class
NXOpen.GeometricAnalysis.
DeviationGaugeBuilderXyzDirectionType
¶ Bases:
object
This enum represents the Deviation Gauge Analysis Object X, Y, Z direction options
Enum Members
Enum Member Enum Member Description X X direction Y Y direction Z Z direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-