DeviationCheckingTypes Enumeration¶
NXOpen.GeometricAnalysis.DeviationChecking.Types is an alias for NXOpen.GeometricAnalysis.DeviationCheckingTypes
-
class
NXOpen.GeometricAnalysis.
DeviationCheckingTypes
¶ Bases:
object
the type of deviation checking to be performed
Enum Members
Enum Member Enum Member Description CurveToCurve check curve/edge to curve/edge deviation CurveToFace check curve/edge to face deviation EdgeToFace check edge to face deviation FaceToFace check face to face deviation EdgeToEdge check edge to edge deviation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-