DeviationCheckingDeviationOptions Enumeration¶
NXOpen.GeometricAnalysis.DeviationChecking.DeviationOptions is an alias for NXOpen.GeometricAnalysis.DeviationCheckingDeviationOptions
-
class
NXOpen.GeometricAnalysis.
DeviationCheckingDeviationOptions
¶ Bases:
object
the deviation type to be shown
Enum Members
Enum Member Enum Member Description NoDeviations show no deviations AllDeviations show all deviations MaximumDistance show maximum distance deviation MinimumDistance show minimum distance deviation MaximumAngle show maximum angle deviation MinimumAngle show minimum angle deviation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-