CurveAnalysisPeaksBuilderDirectionOptionType Enumeration¶
NXOpen.GeometricAnalysis.CurveAnalysisPeaksBuilder.DirectionOptionType is an alias for NXOpen.GeometricAnalysis.CurveAnalysisPeaksBuilderDirectionOptionType
-
class
NXOpen.GeometricAnalysis.
CurveAnalysisPeaksBuilderDirectionOptionType
¶ Bases:
object
Direction option types
Enum Members
Enum Member Enum Member Description NotSet no direction PlaneOfCurve best fit plane SpecifyVector specify vector WorkView work view -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-