CurveAnalysisDisplayShowFlagType Enumeration¶
NXOpen.GeometricAnalysis.CurveAnalysisDisplay.ShowFlagType is an alias for NXOpen.GeometricAnalysis.CurveAnalysisDisplayShowFlagType
-
class
NXOpen.GeometricAnalysis.
CurveAnalysisDisplayShowFlagType
¶ Bases:
object
Show flag types
Deprecated since version NX8.5.0: Use
NXOpen.GeometricAnalysis.CurveAnalysisDisplay.SetShowPole()
,NXOpen.GeometricAnalysis.CurveAnalysisDisplay.SetShowKnot()
,NXOpen.GeometricAnalysis.CurveAnalysisDisplay.SetShowEndPoints()
methods.Enum Members
Enum Member Enum Member Description Pole show pole Comb show comb Inflection show inflection Peak show peak Knot show knot Endpoint show endpoint -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-