GenericMeasureType Enumeration¶
NXOpen.GenericMeasure.Type is an alias for NXOpen.GenericMeasureType
-
class
NXOpen.
GenericMeasureType
¶ Bases:
object
The types for a measurement
Enum Members
Enum Member Enum Member Description MinimumDistance LocalMinimumDistance MaximumDistance ProjectedDistance RadialDistance Length TwoObjectAngle ThreePointAngle FaceProperties MassProperties PointsOnCurves RoutingPathLength DiameterDistance PolarRadius PolarAngle RectangularExtreme PolarArea MinimumSmartDistance MaximumSmartDistance Point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-